Engineering unit converter

BrowseName
EUConverter
SuperType
Converter(Converter)

Properties

Name
BrowseName
DataType
Description
Raw min
RawMin
Minimum input value to convert.
Raw max
RawMax
Maximum input value to convert.
Scaled min
ScaledMin
Minimum value of the converted unit.
Scaled max
ScaledMax
Maximum value of the converted unit.
Source
Source
Dynamic link mode
Mode
(Inherited from Converter)
Is pull
IsPull
(Inherited from Converter)
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.