Digital alarm

Monitors Boolean variables. Activates when the value of the monitored variable is not the normal state value.
BrowseName
OffNormalAlarmController
SuperType
Alarm controller(AlarmController)

Properties

Name
BrowseName
DataType
Description
Normal state value
NormalStateValue
Normal value for the monitored variable. The alarm activates when the value of the variable monitored is different from this.
Enabled
Enabled
(Inherited from Alarm controller)
Active
Active
(Inherited from Alarm controller)
Auto acknowledge
AutoAcknowledge
(Inherited from Alarm controller)
Auto confirm
AutoConfirm
(Inherited from Alarm controller)
Input variable
InputValue
(Inherited from Alarm controller)
Message
Message
(Inherited from Alarm controller)
Severity
Severity
(Inherited from Alarm controller)
Last event
LastEvent
(Inherited from Alarm controller)

Events

OffNormalAlarmType
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.