Alarm controller
Properties
Name | BrowseName | DataType | Description |
---|---|---|---|
Auto acknowledge | AutoAcknowledge | True: when the alarm activates, it is automatically acknowledged and confirmed. False: when the alarm activates, it must be acknowledged by the user. | |
Auto confirm | AutoConfirm | True: when the alarm activates, it is automatically confirmed by the application. False: when the alarm activates, it must be confirmed by the user. | |
Severity | Severity | Level of severity of the alarm, which indicates its priority on a scale from 1 to 1000 (in compliance with the OPC UA standard: 1 = information, 1000 = serious error). | |
Methods
Acknowledge
- BrowseName
- Acknowledge
Name | DataType | Description |
---|---|---|
Confirm
- BrowseName
- Confirm
Name | DataType | Description |
---|---|---|
Add comment
- BrowseName
- AddComment
Name | DataType | Description |
---|---|---|
Provide Feedback