- Getting started
- Using the software
- OPC UA
- Graphic and layout objects
- Developing solutions
- Developing projects with C#
- Application examples
- UI tutorial
- NetLogic tutorial
- Object and variable references
API to create variables
Use C# APIs to create variables in the
FactoryTalk Optix Studio
project and return the corresponding C# objects.The APIs are supplied by the
InformationModel
class, displayed by the FTOptix.HMIProject
module.Provide Feedback