Create remote panel (types)

Create a panel type that will be used on client.
  1. Create a folder for remote panels:
    1. In
      Project view
      , right-click the
      UI
      folder and select
      New
      Folder
      .
    2. Hover-over the folder, select
      Edit
      , and enter
      RemotePanels
      .
  2. Create the main panel:
    1. In
      Project view
      , right-click
      RemotePanels
      and select
      New
      New
      Containers
      Pane
      .
    2. Hover-over the pane, select
      Edit
      , and enter
      MainPanel
      .
  3. Create a panel that displays the Speed variable:
    1. In
      Project view
      , right-click
      RemotePanels
      and select
      New
      New
      Containers
      Pane
      .
    2. Hover-over the pane, select
      Edit
      , and enter
      SpeedPanel
      .
  4. Create a panel that displays the Acceleration variable:
    1. In
      Project view
      , right-click
      RemotePanels
      and select
      New
      New
      Containers
      Pane
      .
    2. Hover-over the pane, select
      Edit
      , and enter
      AccelerationPanel
      .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.