Import and export project elements
Import and export project elements to transfer the elements from one project to another. Depending on the element type, the file formats for import and export are different.
Project Element | File Format |
|---|---|
Micro800 controller programs | M8A |
Micro800 controller user-defined function blocks | M8A |
Micro800 controller user-defined functions | M8A |
Micro800 controller global or local variables | CSV or XLSX |
Micro800 controller user-defined data types | M8A |
Micro800 controller data logs | M8A |
Micro800 controller recipes | M8A |
Micro800 controller configuration - Modbus mapping | CSV |
Micro800 controller configuration - MicroLogix™ mapping | CSV |
Micro800 controller configuration - DNP3 mapping | CSV |
Micro800 controller configuration - DNP3 data set descriptor | M8A |
Micro800 controller configuration - DNP3 data set prototype | M8A |
Provide Feedback