Open an existing project
Use the
Welcome
page or the File
menu to open a user project that was created in FactoryTalk Design Workbench
.You can open multiple sessions of
FactoryTalk Design Workbench
simultaneously, but each project can only be opened in one session.Prerequisites
- Close any open projects.
To open an existing project
- Do one of the following:
- On theWelcomepage, from theRecent Projectslist, select a project.
- On theWelcomepage, selectOpen project, select a project, and then selectOpen.
- From the menu bar, select , select a project, and then selectOpen.
Provide Feedback