Delete a controller
When a controller is deleted from a project, the action is not reversible. All logic programs, variables, and user-defined function blocks associated with the controller are deleted.
To delete a controller
- OpenDelete Devicesby doing one of the following:
- InProject Organizer, right-click the controller, and then selectDelete.
- InProject Organizer, select the controller node, and then select
. - InProject Organizer, select the controller, and then select theDeletekey.
- InDelete Devices, selectDelete.
Provide Feedback