Save a copy of the current project
Use
Save as
to save a copy of the current project with a different project name in the FTDW folder within Documents.To save a copy of the current project
- From the menu bar, select .
- InSave as, enter the project name, and then selectCreate.TIP:Naming conventions are as follows:
- The project name can contain up to 40 characters.
- The project name is restricted to alphanumeric characters and underscores.
- The project name cannot end with an underscore or contain consecutive underscores.
- The project name cannot be reserved words for Windows or Disk Operating System, such as "nul", "aux", "con", "com1", and "lpt1".
After saving a copy of the current project, the original project is closed, and the new project is opened.
Provide Feedback