Create a project
Use the
Welcome
page or the File
menu to create a project. Upon project creation, a directory structure is generated, and the project is saved at the Documents folder.Project naming conventions are as follows:
- The project name can contain up to 40 characters.
- The project name is restricted to alphanumeric characters and underscores.
- The project name cannot end with an underscore or contain consecutive underscores.
- The project name cannot be reserved words for Windows or Disk Operating System, such as "nul", "aux", "con", "com1", and "lpt1".
Prerequisites
- Close any open projects.
To create a project
- OpenNew projectby doing one of the following:
- From theWelcomepage, selectNew project.
- From the menu bar, select .
- InNew project, enter the project name, and then selectCreate.TIP: BecauseAdd device on creationis selected by default,Add deviceopens after project creation. If you do not want to add a device when creating the project, clearAdd device on creation.
- (optional) Add a device to the project:
- InAdd device, select a controller.
- (optional) InSelection, enter the device name, select the device revision, view the device product lifecycle information, and then selectAdd.
Provide Feedback