Close a project
Close a project after completing changes or close a project to open another project.
Prerequisites
- Open a project usingFactoryTalk Design Workbench.
To close a project
- From the menu bar, select .
- (optional) InUnsaved changes, select one of the following:
- Save. Saves the changes and closes the project.
- No. Discards the changes and closes the project.
- Cancel. Reopens the project to make further changes.
Provide Feedback