Interrupt parameters
The supported interrupt parameters vary with the interrupt type.
Interrupt Parameter | Description |
|---|---|
Auto start | Determines whether a user interrupt function configuration is forced without using any ladder logic. It is turned off by default. When turned on, the interrupt is forced without any ladder logic. The interrupt parameter is available for the following interrupt types:
|
Embedded input | Lists the index number of the embedded inputs that are associated with a user interrupt function. Embedded input values for different controller types:
The interrupt parameter is available for EIIs. |
Set point (STI) | Specifies the period between executions of the STI ladder subroutine. If your program contains a large number of rungs for the STI Program Organization Unit and the STI value is small, the interrupts might consume a significant portion, if not all, of your CPU resources. The following problem might occur:
|
Overflow mask (HSCO.MV) | Allows or prohibits an overflow interrupt from occurring. If the bit is clear (0), and an Overflow Reached condition is detected by the high-speed counter (HSC), the HSC user interrupt will not be executed. The Overflow Mask (MV) bit is controlled by the user program and retains its value through a restart. The user program must set and clear the MV bit. HSC modes: 0...9 The interrupt parameter is available for HSC user interrupts. |
Underflow mask (HSCO.MN) | Allows or prohibits am underflow interrupt from occurring. If the bit is clear (0), and an Underflow Reached condition is detected by the HSC, the HSC user interrupt will not be executed. The Underflow Mask (MN) bit is controlled by the user program and retains its value through a restart. The user program must set and clear the MN bit. HSC modes: 2...9 The interrupt parameter is available for HSC user interrupts. |
High preset mask (HSCO.MH) | Allows or prohibits a high preset interrupt from occurring. If the bit is clear (0), and a High Preset Reached condition is detected by the HSC, the HSC user interrupt will not be executed. The High Preset Mask (MH) bit is controlled by the user program and retains its value through a restart. The user program must set and clear the MH bit. HSC modes: 0...9 The interrupt parameter is available for HSC user interrupts. |
Low preset mask (HSCO.ML) | Allows or prohibits a low preset interrupt from occurring. If the bit is clear (0), and a Low Preset Reached condition is detected by the HSC, the HSC user interrupt will not be executed. The Low Preset Mask (ML) bit is controlled by the user program and retains its value through a restart. The user program must set and clear the ML bit. HSC modes: 2...9 The interrupt parameter is available for HSC user interrupts. |
Provide Feedback