UDFB Parameters window
Use the
Parameters
window to:- Create or delete input or output parameters for user-defined function blocks (UDFB) or user-defined functions (UDF).
- Edit the parameters of local variables for UDFBs and UDFs.
- Move a variable up or down in the UDFB or UDF.
UDFs are limited to one output parameter with a modifiable data type. The properties vary with the instruction block type.
Item | Description | Possible Values |
|---|---|---|
Name | Specifies the parameter name. | The naming conventions are as follows:
The naming conventions are based on the IEC-1131 rules for identifiers. |
Data type | Selects the parameter data type. | BOOL, BYTE, DATE, DINT, DWORD, INT, LINT, LREAL, LWORD, REAL, SINT, STRING, TIME, UDINT, UINT, ULINT, USINT, WORD, USER ARRAYS, Defined words, Function blocks. For information about data types, see Data types overview. |
Dimension | Specifies the dimension of the instruction. | Dimension is defined as a positive double integer (DINT) value. For example,
The recommended maximum size limit for a multi-dimensional array is [1..400,1..40]. |
Comment | Contains comments for the parameter. | Free-format text. |
Move up | Moves up the selected parameter. | N/A |
Move down | Moves down the selected parameter. | N/A |
New input | Creates an input parameter. | N/A |
New output | Creates an output parameter. UDFs are limited to one output parameter with a modifiable data type. | N/A |
Delete parameter | Deletes the selected parameter. | N/A |
Provide Feedback