Work in the ladder diagram language editor
Elements are added to the ladder diagram language editor according to the following rules:
- The first element on a rung is added at the position that you selected.
- Subsequent elements are added to the right of the selected element on the rung.
- It is not supported to insert an element to the right of a coil return or jump.
The methods to add elements to the LD program are as follows:
Method | Description |
|---|---|
Ladder editor | Adds, deletes, or copies and pastes elements. |
Toolbox | Adds elements and instructions to the LD program. |
Provide Feedback