Add a rung to the ladder diagram program
Rungs are graphic components of ladder diagram (LD) programs and represent a group of circuit elements that activate a coil.
To add a rung to the ladder diagram program
- Do one of the following:
- FromToolbox, drag
to a valid location in the language editor.
indicates a valid dropping location. - In the LD language editor, right-click theEndrung, and then selectAdd element.
Provide Feedback