Work with elements in language editors
Use the language editors to manage individual or multiple elements for Micro800 controller programs. The selected elements are highlighted in blue.
To | Do this |
|---|---|
Select an individual element | Select the element in the language editor. |
Select multiple elements | Do one of the following:
The elements must be within the same rung. |
Insert an element to a language editor | From Toolbox , drag the element to the language editor. |
Delete elements | Do one of the following:
Deleting a variable does not delete the variable from the dictionary. |
Move elements | In the language editor, select one or more elements, and then drag the elements to another location within the language editor. You can select multiple elements only within the same rung. |
Resize elements | Select the element, and then drag the element handle until it reaches the desired size. |
Open the local variables grid | In the language editor, select . |
Show or hide grids in function block diagram programs | In the language editor, select or . |
Zoom in or zoom out | Do one of the following:
|
Provide Feedback
.
or
.
or
.