Trig Functions
Use Trig Functions to evaluate arithmetic operations using trigonometric operations.
Function | Description |
|---|---|
Calculates the arc-cosine of a Real value. | |
Calculates the arc-cosine of a Long Real value. | |
Calculates the arcsine of a Real value. | |
Calculates the arcsine of a Long Real value. | |
Calculates the arctangent of a Real value. | |
Calculates the arctangent of a Long Real value. | |
Calculates the cosine of a Real value. | |
Calculates the cosine of a Long Real value. | |
Calculates the sine of a Real value. | |
Calculates the sine of a Long Real value. | |
Calculates the tangent of a Real value. | |
Calculates the tangent of a Long Real value. |
Provide Feedback