CHAR (ASCII code to string character)
The CHAR instruction returns a one-character string for an ASCII code. ASCII code -> character.
Languages supported: Function block diagram, ladder diagram, structured text.
This instruction applies to the Micro810, L20E, L50E, and L70E controllers.
CHAR

Parameter | Parameter Type | Data Type | Description |
|---|---|---|---|
EN | Input | BOOL | Instruction enable.
Applies to ladder diagram programs. |
Code | Input | DINT | ASCII code in set to [0 .. 255]. |
CHAR | Output | STRING | One-character string. The character has the ASCII code given in input code. |
ENO | Output | BOOL | Enable output. Applies to ladder diagram programs. |
CHAR examples
CHAR function block diagram example

CHAR ladder diagram example

CHAR structured text example

(* ST Equivalence: *) Display := CHAR ( value + 48 ); (* value is in set [0..9] *) (* 48 is the ascii code of '0' *) (* result is one character string from '0' to '9' *)
Results

Provide Feedback