Socket error codes
ErrorID Code | SubErrorID Code | Error Description | Corrective Action |
|---|---|---|---|
0 | The Socket instruction successfully completed operation. | ||
1 | The Socket instruction is pending. | ||
2 | The Socket Instance is not available. | Confirm that the Socket Instance is not deleted or the Timeout value exceeded. | |
3 | The SOCKET_DELETEALL operation is ongoing. | Wait for the pending SOCKET_DELETEALL operation to complete. | |
4 | 1 | Illegal Parameter, Invalid Channel. | No action. Reserved for future use. |
4 | 2 | Illegal Parameter, Invalid Socket IP Address.
| Change to a valid IP address. |
4 | 3 | Illegal Parameter, Invalid Socket Port Address. Error occurs when the following Ports are specified in SOCKET_CREATE, SOCKET_OPEN, or SOCKET_WRITE:
| Change the Port Address. |
4 | 4 | Illegal Parameter, Invalid Socket Type. Valid Socket Types are:
| Change Socket Type. |
4 | 5 | Illegal Parameter, Invalid Socket Timeout value. Valid Timeout values are:
| Change the Timeout value to a valid value. |
4 | 6 | Illegal Parameter, Invalid Socket Instance.
| Use the Instance Number returned in SOCKET_CREATE and SOCKET_ACCEPT instructions after successful execution. |
4 | 7 | Illegal Parameter, Invalid Array Length. | Increase the size of the array used to contain the Socket read and write data. |
4 | 8 | Illegal Parameter, Invalid Array Dimension. | Use a one-dimensional array to contain the Socket read and write data. |
5 | Socket request to cancel operation. Error occurs when:
| Restart the Socket operation based on Socket Type. Refer to the respective State Machine to restart Socket operation. | |
6 | 1 | Illegal Socket Sequence, Socket Open Operation in progress or Connected. Error occurs when:
| Use single SOCKET_OPEN execution for respective Socket Instance. Do not perform SOCKET_ACCEPT operation for same socket instance. |
6 | 2 | Illegal Socket Sequence, Socket Accept Operation In progress or Connected. Error occurs when:
| Use single SOCKET_ACCEPT execution for respective Socket Instance. Do not perform SOCKET_OPEN operation for same socket instance. |
6 | 3 | Illegal Socket Sequence, Socket configured as TCP Client. | |
6 | 4 | Illegal Socket Sequence, Socket configured as TCP Server. | |
6 | 5 | Illegal Socket Sequence, Socket is Connected. | Make sure that the Socket is not already connected with a remote device before executing SOCKET_OPEN or SOCKET_ACCEPT again. |
6 | 6 | Illegal Socket Sequence, Socket configured as UDP. | Make sure that UDP Socket Instances are not used with SOCKET_ACCEPT. |
6 | 7 | Illegal Socket Sequence, Socket is not connected. | Confirm that the Socket is connected with the target. |
7 | Socket Instance Timeout. | Configure Timeout values for SOCKET_ACCEPT, SOCKET_OPEN, SOCKET_READ, and SOCKET_WRITE accordingly. | |
8 | The Socket module is not initialized. | Make sure that the Ethernet Link is Enabled or Ethernet Cable of Controller is connected to the Network or resolve Controller IP Address conflict. | |
9 | 1 | Socket Instruction Fatal Error, Socket Instance Missing. | |
9 | 2 | Socket Instruction Fatal Error, Invalid Socket Instance. | |
9 | 3 | Socket Instruction Fatal Error, Invalid Lock Socket Instance. | |
9 | 4 | Socket Instruction Fatal Error, Invalid Socket Type. | |
9 | 5 | Socket Instruction Fatal Error, Missing Cancel Handler. | |
10 | 1 | Socket background processing Error, Address in Use. | |
10 | 2 | Socket background processing Error, UDP Received a Large Packet and the Packet is larger than Socket Read length. | Make sure the SOCKET_READ Length is equal to greater than the received packet size. Max read size is recommended. Max size for SOCKET_READ is 256. |
10 | 3 | Socket background processing Error, TCP Receive Large packet. Packet received is larger than the Socket Read length. | Make sure the SOCKET_READ Length is equal to greater than the received packet size. Because client might send up to the receive window size of 256, 256 is recommended. |
10 | 4 | Socket background processing Error, Received RST or Disconnect from Remote Device. | Restart Controller TCP Client or Server as shown in the State Diagram. Verify the Target device that sent RST and make sure that the Target is restarted with correct state. |
10 | 5 | Socket background processing Error, UDP Packet received from different device, drop packet. Reserved for future. | |
10 | 6 | Socket background processing Error, Queue is full. Error occurs when:
| Wait for SOCKET_READ and SOCKET_WRITE queue availability for respective Socket instance. |
10 | 7 | Socket background processing Error, SOCKET_READ Parameter change (Length, Offset, Data Array Size, and Data Array Variable). | When the SOCKET_READ state is BUSY, do not modify the input parameters. |
11 | 1 | Socket background processing Fatal Error, Missing data pointer. | |
11 | 2 | Socket background processing Fatal Error, Missing Session Pointer. | |
11 | 3 | Socket background processing Fatal Error, Invalid TCP or UDP Socket pointer. | |
11 | 4 | Socket background processing Fatal Error, Invalid Socket Instance Type. | |
11 | 5 | Socket background processing Fatal Error, Socket Instance Missing. | |
11 | 6 | Socket background processing Fatal Error, Invalid Socket Instance. | |
11 | 7 | Socket background processing Fatal Error, Invalid Socket State. | |
11 | 8 | Socket background processing Fatal Error, Invalid Socket Type. | |
11 | 9 | Socket background processing Fatal Error, TCP delete Failure. | |
11 | 10 | Socket background processing Fatal Error, UDP delete Failure. | |
128 | 1 | No packet available for disconnect message. | |
128 | 2 | Not enough room to pre-pend the TCP header. | |
128 | 3 | Packet append pointer is invalid. | |
128 | 7 | Invalid Socket pointer. | |
128 | 10 | Invalid type-of-service, fragment, or time-to-live option. | |
128 | 17 | Invalid caller for this service. | |
128 | 18 | Packet is not valid. | |
128 | 20 | This component has not been enabled. | |
128 | 21 | This component has already been enabled. | |
128 | 22 | Listening is not enabled for the specified port. | |
128 | 26 | Requested suspension was aborted. | |
128 | 33 | Invalid server IP Address. | |
128 | 34 | This socket is bound to another port. | |
128 | 35 | Port is bound to a different socket. | |
128 | 36 | Socket is not bound. | |
128 | 38 | The Socket was unbound while suspended waiting for a receive packet. | |
128 | 39 | Socket was not created. | |
128 | 51 | No additional listen request structures are available. | |
128 | 52 | There is already an active listen request for this port. | |
128 | 53 | Socket is not in a closed state. | |
128 | 54 | The server socket supplied is not in a listen state. | |
128 | 55 | No wait time was specified, the connection attempt is in progress. | |
128 | 56 | Connection failed. | |
128 | 57 | Request is greater than the receiver's advertised window size in bytes. | |
128 | 64 | Another thread is suspended. Only one thread is allowed. | |
128 | 65 | Disconnect failed to complete within the Timeout period. | |
128 | 66 | Socket is bound. | |
128 | 69 | No available Port. | |
128 | 70 | Invalid Port. | |
128 | 71 | There is already a valid Socket pointer for this port or the specified port does not have an active listen request. | |
128 | 72 | Same as NX_SUCCESS, except a queued connection request was processed during this call. | |
128 | 73 | TCP Transmit Queue Exceeded Error. |
Provide Feedback