Program control instruction
Use the program control instruction to control instructions simultaneously from a user program and from an operator interface device.
Instruction | Description |
|---|---|
Disables a rung. | |
Functions as a placeholder. | |
Reads the user program checksum, from the controller or the memory module. | |
Suspends the execution of the Micro800 controller. | |
Stops the current cycle of the user program scan. | |
Reads the status data block for the Micro800 controller. |
Provide Feedback