SCL (scaler with alarm)
The SCL instruction converts an unscaled REAL input value to a REAL floating point value in engineering units and includes alarming and limiting of the output.
Languages supported: Function block diagram, ladder diagram, structured text.
This instruction applies to the L20E, L50E, and L70E controllers.
SCL

Parameter | Parameter Type | Data Type | Description |
|---|---|---|---|
Enable | Input | BOOL |
|
In | Input | REAL | The analog signal input. Valid = any float Default = 0.0 |
InRawMax | Input | REAL | The maximum value attainable by the input to the instruction. If InRawMax<= InRawMin, the instruction sets the appropriate bit in Status and Error. ErrorID are updated. Out updating stops. Valid = InRawMax > InRawMin Default =0.0 |
InRawMin | Input | REAL | The minimum value attainable by the input to the instruction. If InRawMin >= InRawMax, the instruction sets the appropriate bit in Status and Error. ErrorID are updated. Out updating stops. Valid = InRawMin < InRawMax Default = 0.0 |
InEUMax | Input | REAL | The scaled value of the input corresponding to InRawMax. Valid = any real value Default = 0.0 |
InEUMin | Input | REAL | The scaled value of the input corresponding to InRawMin. Valid = any real value Default = 0.0 |
Limiting | Input | BOOL | Limiting selector. TRUE: Out is limited between InEUMin and InEUMax. |
Done | Output | BOOL | Indicates when the operation is completed.
|
EnableOut | Output | BOOL | Indicates if the instruction is enabled. Sets to False if Out overflows. |
Out | Output | REAL | Represents the scaled value of the analog input. |
MaxAlarm | Output | BOOL | The maximum input alarm indicator. This value is set to TRUE when Input > InRawMax. |
MinAlarm | Output | BOOL | The minimum input alarm indicator. This value is set to TRUE when Input < InRawMin. |
Status | Output | DINT | Status of the Function block. InstructFault (Status.0). It will be set when detected the instruction's execution errors. This is not the minor or major controller error. Check the remaining status bits to determine what has occurred. InRawRangeInv (Status.1) InRawMin >= InRawMax Status.3 to Status.31 are reserved for future usage and their value is 0. |
Error | Output | BOOL | Indicates the existence of an error condition.
|
ErrorID | Output | BOOL | A unique numeric that identifies the error. The errors are defined in the error codes. |
ErrorID Code | Error Description |
|---|---|
1 | InRawMax<= InRawMin |
SCL examples
SCL function block diagram example

SCL ladder diagram example

SCL structured text example

Provide Feedback