Configure auto-tuning
Use these general steps when implementing auto-tuning using the IPIDCONTROLLER function.
Step | Description | Example |
|---|---|---|
1 | Reset SetPoint to zero. | ![]() |
2 | Switch Auto mode to False. | ![]() |
3 | Set Gains parameters. | ![]() |
4 | Set AutoTune parameters. | ![]() |
5 | Set Initialize and AutoTune to True. | ![]() |
6 | Notice the Output changes to the value of Load when you set AutoTune to True. | ![]() |
7 | Observe the process value rises quickly until it gets closer to its saturation point. | ![]() |
8 | Observe the stabilization of the process value and its fluctuation. | ![]() ![]() |
9 | Set the deviation. | ![]() |
10 | Set Initialize to False. | ![]() |
11 | Controller starts auto-tuning. Wait for ATWarning to become 2. | ![]() |
12 | Set AutoTune to False. | ![]() |
13 | Observe the tuned values appear in OutGains. | ![]() |
14 | Transfer parameter from OutGain to My_Gains. | ![]() |
15 | Observe the controller is updated with the with the tuned gain parameter. | ![]() |
Provide Feedback