MC_ReadAxisError (motion control read axis error)
The MC_ReadAxisError instruction reads the axis errors not related to the motion control instruction blocks.
When an axis is in a Disabled state, MC_ReadAxisError might or might not get a nonzero Error ID for the axis because a Disabled axis can contain errors or be error-free.
Languages supported: Function block diagram, ladder diagram, structured text.
This instruction applies to the L50E and L70E controllers that support motion control.
MC_ReadAxisError

Parameter | Parameter Type | Data Type | Description |
|---|---|---|---|
EN | Input | BOOL | Instruction block enable.
Applies only to ladder diagram programs. |
AxisIn | Input | AXIS_REF FB_AXIS_REF | Use the AXIS_REF data type parameters to define AxisIn. For an FB_Axis (feedback axis), use the FB_AXIS_REF data type to define AxisIn. |
Enable | Input | BOOL |
|
ENO | Output | BOOL | Enable output. Applies only to ladder diagram programs. |
Axis | Output | AXIS_REF | Axis output is read-only in ladder diagram programs. The Axis output parameters are defined in the FB_AXIS_REF data type. |
Valid | Output | BOOL |
|
Busy | Output | BOOL |
|
Error | Output | BOOL | Indicates that an error occurred.
|
ErrorID | Output | UINT | A unique numeric that identifies the error. The errors for this instruction are defined in motion control function block error IDs. |
AxisErrorID | Output | UINT | A unique numeric that identifies the axis error. The errors for this instruction are defined in Motion control function block error IDs. |
MC_ReadAxisError examples
MC_ReadAxisError function block diagram example

MC_ReadAxisError ladder diagram example

MC_ReadAxisError structured text example

Results


Provide Feedback