Trimpot ID definition
The following table describes the Trimpot ID definition used in the TRIMPOT_READ instruction.
Output Selection | Bit | Description |
|---|---|---|
Trimpot ID definition | 15 - 13 | Module type of trimpot:
|
12 - 8 | Slot ID of the module:
| |
7 - 4 | Trimpot type:
| |
3 - 0 | Trimpot ID inside the module:
The trimpot ID starts from 0. |
Provide Feedback