MM_INFO (memory module information)
The MM_INFO instruction reads memory module header information. When a memory module is not present, all values return zero (0).
Languages supported: Function block diagram, ladder diagram, structured text.
This instruction applies to the
Micro810
, L20E, L50E, and L70E controllers.MM_INFO

Parameter | Parameter Type | Data Type | Description |
|---|---|---|---|
Enable | Input | BOOL | Instruction block enable.
|
ENO | Output | BOOL | Enables output. Applies to ladder diagram programs. |
MM_INFO examples
MM_INFO function block diagram example

MM_INFO ladder diagram example

MM_INFO structured text example

Results - Controllers using 2080-MEMBAK-RTC

Results - Controllers using an SD card

Provide Feedback