Review the complete program results
The following example shows the complete MSG_CIPSYMBOLIC messaging program after it has executed.
Global variable grid of the MSG_CIPSYMBOLIC messaging program

Ladder diagram of the MSG_CIPSYMBOLIC messaging program

Controller B results
The following two images show the values for Controller B before and after the messaging program is executed.
- Before the program executes

- After the program executes

Provide Feedback