Message timeout
The following table describes how timers for inUcmmTimeout and ConnMsgTimeout parameters behave based on message requests and status.
Action | Result |
|---|---|
Message is enabled. | UcmmTimeout timer is activated. |
CIP Connection is requested. | ConnMsgTimeout timer is activated. |
ConnMsgTimeout timer is active. | UcmmTimeout timer is disabled.
Applicable for Ethernet/IP. |
Connection request is completed. | UcmmTimeout timer is reactivated.
Applicable for Ethernet/IP. |
Provide Feedback