Message execution timing diagram (PCCC configuration error)
The following table describes the message conditions and bit status for each execution step identified in the timing diagram when a PCCC configuration error occurs during execution.
Step | Message Description | Bit Status |
|---|---|---|
1 | Rung condition goes TRUE. Message execution is enabled. | EN bit is set. |
2 | Message buffer is acquired. | EW bit is set. |
3 | Invalid elements exist in PCCCCfg. | ER bit is set to 1 before ST bit is set to 1. EW and ST bits do not change. |
4 | As rung condition goes FALSE. | EN, EW, and ER bits are cleared. |
Error condition diagram
Error condition when changing the number of elements in PCCCCfg to an invalid number 17

Provide Feedback