Message execution process (Error)
The following table describes the message conditions and bit status for each execution step identified in the timing diagram when an error occurs during execution.
Step | Message Description | Bit Status |
|---|---|---|
1 | Rung condition goes TRUE. Message execution is enabled. | EN bit is set. All other bits are cleared. |
2 | Message buffer is acquired. | EW bit is set. |
3 | Message transmission starts. | EW bit is cleared. ST bit is set. |
4 | Message transmission times out. | EW and ST bits do not change. |
4-6 | As rung condition goes FALSE. | EN bit is cleared. ER bit is set. |
Provide Feedback