UIC (clear interrupt lost bit)
The UIC instruction clears the lost bit for the selected user interrupt(s).
Languages supported: Function block diagram, ladder diagram, structured text.
This instruction applies to the L20E, L50E, and L70E controllers.
UIC

Parameter | Parameter Type | Data Type | Description | |
|---|---|---|---|---|
Enable | Input | BOOL | Instruction enable.
| |
IRQType | Input | UDINT | Use the STI defined words.
|
|
UIC | Output | BOOL | Rung status (same as Enable). | |
UIC examples
UIC function block diagram example

UIC ladder diagram example

UIC structured text example

Results

Provide Feedback