Instruction set in alphabetical order
The following table lists the
Micro800
controller instructions available in FactoryTalk Design Workbench
.Instruction | Category | Type | Description |
|---|---|---|---|
SUB | Math | Operator | Subtracts one Integer, Real, or Time value from another Integer, Real or, Time value. |
MUL | Math | Operator | Multiplies two or more Integer or Real values. |
DIV | Math | Operator | Division of two Integer or Real values. |
ADD | Math | Operator | Adds two or more Integer, Real, Time, or String values. |
LT | Compare | Operator | Compares Integer, Real, Time, Date, and String input values to determine whether the first is less than the second. |
LE | Compare | Operator | Compares Integer, Real, Time, Date, and String input values to determine whether the first is less than or equal to the second. |
NE | Compare | Operator | Compares Integer, Real, Time, Date, and String input values to determine whether the first is not equal to the second. |
EQ | Compare | Operator | Tests whether one value is equal to another. |
GT | Compare | Operator | Compares Integer, Real, Time, Date, and String input values to determine whether the first is greater than the second. |
GE | Compare | Operator | Compares Integer, Real, Time, Date, and String input values to determine whether the first is greater than or equal to the second. |
ABL | Serial Port | Function block | Counts the number of characters in the buffer up to and including end of line character. |
ABS | Math | Function | Returns the absolute value of a Real value. |
ACB | Serial Port | Function block | Counts the total number of characters in the buffer. |
ACL | Serial Port | Function block | Clears the receive and transmit buffers. |
ACOS | Trig Functions | Function | Calculates the arc-cosine of a Real value. |
ACOS_LREAL | Trig Functions | Function | Calculates the arc-cosine of a Long Real value. |
AFI | Program Control | Function | Temporarily disables a rung when debugging. |
AHL | Serial Port | Function block | Sets or resets modem handshake lines. |
AND | Logical | Operator | Performs a Boolean AND operation between two or more values. |
AND_MASK | Logical | Function | Performs a bit to bit AND between two Integer values. |
ANY_TO_BOOL | Conversion | Function | Converts a non-Boolean value to a Boolean value. |
ANY_TO_BYTE | Conversion | Function | Converts a value to a Byte. |
ANY_TO_DATE | Conversion | Function | Converts a String, Integer, Real, or Time data type to the Date data type. |
ANY_TO_DINT | Conversion | Function | Converts a value to a Double Integer. |
ANY_TO_DWORD | Conversion | Function | Converts a value to a Double Word value. |
ANY_TO_INT | Conversion | Function | Converts a value to an Integer. |
ANY_TO_LINT | Conversion | Function | Converts a value to a Long Integer. |
ANY_TO_LREAL | Conversion | Function | Converts a value to a Long Real. |
ANY_TO_LWORD | Conversion | Function | Converts a value to a Long Word. |
ANY_TO_REAL | Conversion | Function | Converts a value to a Real. |
ANY_TO_SINT | Conversion | Function | Converts a value to a Short Integer. |
ANY_TO_STRING | Conversion | Function | Converts a value to a String. |
ANY_TO_TIME | Conversion | Function | Converts a value to the Time data type. |
ANY_TO_UDINT | Conversion | Function | Converts a value to an Unsigned Double Integer. |
ANY_TO_UINT | Conversion | Function | Converts a value to an Unsigned Integer. |
ANY_TO_ULINT | Conversion | Function | Converts a value to an Unsigned Long Integer. |
ANY_TO_USINT | Conversion | Function | Converts a value to an Unsigned Short Integer. |
ANY_TO_WORD | Conversion | Function | Converts a value to a Word. |
ARD | Serial Port | Function block | Reads characters from the input buffer and places them into a string. |
ARL | Serial Port | Function block | Reads one line of characters from the input buffer and places them into a string. |
ASCII | ASCII String | Function | Returns the ASCII code for characters in a string. Character -> ASCII code. |
ASIN | Trig Functions | Function | Calculates the arcsine of a Real value. |
ASIN_LREAL | Trig Functions | Function | Calculates the arcsine of a Long Real value. |
ATAN | Trig Functions | Function | Calculates the arctangent of a Real value. |
ATAN_LREAL | Trig Functions | Function | Calculates the arctangent of a Long Real value. |
AVE | File/Array | Function block | Calculates a running average over a number of a defined samples. |
AWA | Serial Port | Function | Writes a string with two appended (user-configured) characters to an external device. |
AWT | Serial Port | Function | Writes characters from a source string to an external device. |
BSL | File/Shift | Function block | Shifts a bit in an array element to the left. |
BSR | File/Shift | Function block | Shifts a bit in an array element to the right. |
CHAR | ASCII String | Function | Returns a one character string for an ASCII code. ASCII code -> character. |
COM_IO_WDOG | Communications | Function block | Monitors communication to the controller. |
COP | Move/Copy | Function block | Copies the binary data in the source element to the destination element. |
COS | Trig Functions | Function | Calculates the cosine of a Real value. |
COS_LREAL | Trig Functions | Function | Calculates the cosine of a Long Real value. |
CTD | Timer/Counter | Function | Counts integers from a given value down to 0, one by one. |
CTU | Timer/Counter | Function | Counts integers from 0 up to a given value, one by one. |
CTUD | Timer/Counter | Function | Counts integers from 0 up to a given value, one by one, or from a given value down to 0, one by one. |
DELETE | ASCII String | Function | Deletes characters from a string. |
DERIVATE | Advanced Math | Function block | Differentiation of a real value over a defined cycle time. |
DLG | Data Log/Recipe | Function block | Writes variable values from the run-time engine into a Data Logging File on an SD card. |
DOY | Date Time | Function | Turns on an output if the value of the real-time clock is in the range of the Year Time setting. |
EXPT | Advanced Math | Function | Calculates the Real value of a base number raised to the power of the Integer exponent. |
OSF | Bit | Function block | Detects a falling edge of a Boolean variable. |
FFL | File/Shift | Function block | Loads 8-bit, 16-bit, 32-bit, or 64-bit data into a user-created array called a FIFO stack. |
FFU | File/Shift | Function block | Unloads 8-bit, 16-bit, 32-bit, or 64-bit data from a user-created array called a FIFO (first in first out) stack in the same order data was loaded using the FFL instruction. |
FIND | ASCII String | Function | Locates and provides the position of sub-strings within strings. |
HSC | HSC | Function block | Applies high presets, low presets, and output source values to the high-speed counter. |
HSC_SET_STS | HSC | Function block | Manually sets or resets the HSC counting status. |
HSCE | HSC | Function block | Starts, stops, and reads the accumulator value. |
HSCE_CFG | HSC | Function block | HSCE_CFG is the high-speed counter configuration. |
HSCE_CFG_PLS | HSC | Function block | HSCE_CFG_PLS is the high-speed counter PLS configuration. |
HSCE_READ_STS | HSC | Function block | HSCE_READ_STS reads high-speed counter status. |
HSCE_SET_STS | HSC | Function block | Manually sets or resets high-speed counter status. |
HYSTER | Process | Function block | Boolean hysteresis on difference of reals. |
IIM | Input/Output | Function block | Updates inputs prior to normal output scan. |
INSERT | ASCII String | Function | Inserts sub-strings at user-defined positions within strings. |
INTEGRAL | Advanced Math | Function block | Integrates a real value during the defined cycle time. |
IOM | Input/Output | Function block | Updates outputs prior to normal output scan. |
IPIDCONTROLLER | Process | Function block | Configures and controls the inputs and outputs used for the Proportional Integral Derivative (PID) logic. |
KEY_READ | LCD | Function block | Reads the Key status on the optional LCD module when the user display is active.
Available for Micro810 controllers. |
KEY_READ_REM | LCD | Function block | Reads the Key status on the optional Remote LCD module when the user display is active.
Available for L20E, L50E, and L70E controllers. |
LCD | LCD | Function | Displays a string or number on an LCD screen.
Available for Micro810 controllers. |
LCD_BKLT_REM | LCD | Function | Sets the Remote LCD backlight parameters in a user program. |
LCD_REM | LCD | Function | Displays user-defined messages for the Remote LCD. |
LEFT | ASCII String | Function | Extracts characters from the left side of a string. |
LFL (LIFO load) | File/Shift | Function block | Loads 8-bit, 16-bit, 32-bit, or 64-bit data into a user-created array called a LIFO stack. |
LFU (LIFO unload) | File/Shift | Function block | Unloads 8-bit, 16-bit, 32-bit, or 64-bit data from a user-created array called a LIFO (last in first out) stack in the same order data was loaded using the LFL instruction. |
LIM | Compare | Function block | An alarm with hysteresis on a Real value for high and low limits. |
LIMIT | Compare | Function | Restricts integer values to a given interval. |
LOG | Advanced Math | Function | Calculates the logarithm (base 10) of a Real value. |
MAX | Compare | Function | Calculates the maximum of two integer values. |
MC_AbortTrigger | Motion Event | Function block | Aborts Motion function blocks that are connected to trigger events. |
MC_Halt | Motion Move | Function block | Commands a controlled motion stop under normal operating conditions. |
MC_Home | Motion Move | Function block | Commands the axis to perform the <search home> sequence. |
MC_MoveAbsolute | Motion Move | Function block | Commands a controlled motion to a specified absolute position. |
MC_MoveRelative | Motion Move | Function block | Commands a controlled motion of a specified distance relative to the actual position at the time of the execution. |
MC_MoveVelocity | Motion Move | Function block | Commands a never ending controlled motion at a specified velocity. |
MC_Power | Motion State | Function block | Controls the power stage, ON or OFF. |
MC_ReadActualPosition | Motion Move | Function block | Returns the actual position of the feedback axis. |
MC_ReadActualVelocity | Motion Move | Function block | Returns the actual velocity of the feedback axis. |
MC_ReadAxisError | Motion State | Function block | Reads the axis errors not related to the Motion control instruction blocks. |
MC_ReadBoolParameter | Motion Config | Function block | Returns the value of a vendor specific parameter of type BOOL. |
MC_ReadParameter | Motion Config | Function block | Returns the value of a vendor specific parameter of type Real. |
MC_ReadStatus | Motion State | Function block | Returns the status of the axis with respect to the motion currently in progress. |
MC_Reset | Motion State | Function block | Transitions the axis state from Error Stop to Standstill by resetting all internal axis-related errors. |
MC_SetPosition | Motion Move | Function block | Shifts the coordinate system of an axis by manipulating the actual position. |
MC_Stop | Motion Move | Function block | Commands a controlled motion stop and transfers the axis state to Stopping. |
MC_TouchProbe | Motion Event | Function block | Records an axis position at a trigger event. |
MC_WriteBoolParameter | Motion Config | Function block | Modifies the value of a vendor specific parameter of type Bool. |
MC_WriteParameter | Motion Config | Function block | Modifies the value of a vendor specific parameter of type Real. |
MID | ASCII String | Function | Extracts characters from the middle of a string. |
MIN | Compare | Function | Calculates the minimum of two integer values. |
MLEN | ASCII String | Function | Calculates the length of a string. |
MM_INFO | Module | Function block | Reads memory module header information. |
MOD | Math | Function | Performs a Module calculation on Integer values. |
MODULE_INFO | Module | Function block | Reads module information from a plug-in module or an expansion module. |
MOVE | Move/Copy | Operator | Assigns the input value to the output. |
MSG_CIPGENERIC | Messaging | Function | Sends a CIP generic explicit message. |
MSG_CIPSYMBOLIC | Messaging | Function | Sends a CIP symbolic explicit message. |
MSG_MODBUS | Messaging | Function | Sends a Modbus message. |
MSG_MODBUS2 | Messaging | Function | Sends a MODBUS/TCP message over an Ethernet Channel. |
MSG_PCCC | Messaging | Function | Sends a PCCC message over an Ethernet channel or a serial port. |
MUX4B | Logical | Function | Multiplexer between four BOOL inputs, outputs a BOOL value. |
MUX8B | Logical | Function | Multiplexer between eight BOOL inputs, outputs a BOOL value. |
Neg | Math | Operator | Converts a value to a negative. |
NOP | Program Control | Function | Functions as a placeholder. |
NOT | Logical | Operator | Converts Boolean values to negated values. |
NOT_MASK | Logical | Function | Integer bit-to-bit negation mask, inverts a parameter value. |
OR | Logical | Operator | Boolean OR of two or more values. |
OR_MASK | Logical | Function | Integer OR bit-to-bit mask, turns bits on. |
PID | Process | Function block | An output instruction that controls physical properties such as temperature, pressure, liquid level, or flow rate using process loops. |
PLUGIN_INFO | Module | Function block | Gets module information from a generic plug-in module (excluding Memory Module). |
PLUGIN_READ | Module | Function block | Reads data from a generic plug-in module (excluding Memory Module). |
PLUGIN_RESET | Module | Function block | Resets a generic plug-in module, hardware reset (excluding Memory Module). |
PLUGIN_WRITE | Module | Function block | Writes data to a generic plug-in module (excluding Memory Module). |
EXPT_REAL | Advanced Math | Function | Calculates the value of a Real number raised to a power of the Real exponent. |
PWM | Input/Output | Function block | Turns the PWM (Pulse Width Modulation) output for a configured PWM channel ON or OFF. |
OSR | Bit | Function block | Detects a rising edge of a Boolean variable. |
RAND | Advanced Math | Function | Calculates random integer values from a defined range. |
RCP | Data Log/Recipe | Function block | Reads and writes recipe data to and from an SD memory card. |
REPLACE | ASCII String | Function | Replaces parts of a string with new sets of characters. |
RHC | Timer/Counter | Function | Reads the high-speed clock. |
RIGHT | ASCII String | Function | Extracts characters from the right side of a string. |
ROL | File/Shift | Function | For 32-bit integers, rotates integer bits to the left. |
ROR | File/Shift | Function | For 32-bit integers, rotates integer bits to the right. |
RPC | Program Control | Function | Reads user program checksum. |
RS | Logical | Function block | Resets dominant bistable. |
RTC_READ | Date Time | Function block | Reads the real-time clock (RTC) module information. |
RTC_SET | Date Time | Function block | Sets RTC (real-time clock) data to the RTC module information. |
RTO | Timer/Counter | Function block | Retentive timing. Increases an internal timer when input is active, but does not reset the internal timer when input changes to inactive. |
SCALER | Input/Output | Function block | Scales the input value according to output range. |
SCL | Process Control | Function block | Converts an unscaled input value to a floating point value in engineering units. |
SHL | File/Shift | Function | For 32-bit integers, moves integers to the left and places 0 in the least significant bit. |
SHR | File/Shift | Function | For 32-bit integers, moves integers to the right and places 0 in the most significant bit. |
SIN | Trig Functions | Function | Calculates the sine of a Real value. |
SIN_LREAL | Trig Functions | Function | Calculates the sine of a Long Real value. |
SOCKET_ACCEPT | Sockets | Function block | Accepts a TCP connection request from a remote destination and returns a socket instance used to send and receive data on the newly created connection. |
SOCKET_CREATE | Sockets | Function block | Creates an instance of the socket and returns an instance number that is used as an input in any follow-on socket operations. |
SOCKET_DELETE | Sockets | Function block | Deletes a created socket instance. |
SOCKET_DELETEALL | Sockets | Function block | Deletes all created socket instances. |
SOCKET_INFO | Sockets | Function block | Returns information for the socket such as error codes and execution status. |
SOCKET_OPEN | Sockets | Function block | Opens the connection for the specified destination address for Transmission Control Protocol (TCP) connections. For User Datagram Protocol (UDP) connections, associates a destination IP address and port number with the specified socket. |
SOCKET_READ | Sockets | Function block | Reads data on a socket. |
SOCKET_WRITE | Sockets | Function block | Sends data on a socket. |
SQRT | Advanced Math | Function | Calculates the square root of a Real value. |
SR | Logical | Function block | Sets dominant bistable. |
STACKINT | File/Shift | Function block | Manages stack of integers. |
STIS | Interrupt | Function | Starts the selected timed user interrupt (STI ) timer from the control program rather than starting automatically. |
SUS | Program Control | Function block | Suspends the execution of the Micro800 controller. |
SYS_INFO | Program Control | Function block | Reads the status data block for the Micro800 controller. |
TAN | Trig Functions | Function | Calculates the tangent of a Real value. |
TAN_LREAL | Trig Functions | Function | Calculates the tangent of a Long Real value. |
TDF | Date Time | Function | Computes the time difference between TimeA and TimeB. |
TND | Program Control | Function | Stops the current cycle of the user program scan. |
TOF | Timer/Counter | Function block | Off-delay timing. Increases an internal timer up to a given value. |
TON | Timer/Counter | Function block | On-delay timing. Increases an internal timer up to a given value. |
TONOFF | Timer/Counter | Function block | Delays turning on an output on a true rung, and then delays turning off the output on the false rung. |
TOW | Date Time | Function | Turns on an output if the value of the real-time clock is in the range of the Time of Week setting. |
TP | Timer/Counter | Function block | Pulse timing. On a rising edge, increases an internal timer up to a given value. |
TRIMPOT_READ | Module | Function block | Reads the trimpot value from a specific trimpot. |
TRUNC | Math | Function | Truncates Real values, leaving just the Integer. |
TTABLE | Logical | Function | Provides the value of the output based on the combination of inputs. |
UIC | Interrupt | Function | Clears the lost bit for the selected user interrupt. |
UID | Interrupt | Function | Disables a specific user interrupt. |
UIE | Interrupt | Function | Enables a specific user input. |
UIF | Interrupt | Function | Flushes or removes a pending user input. |
XOR | Logical | Operator | Boolean exclusive OR of two values. |
XOR_MASK | Logical | Function | Integer exclusive OR bit-to-bit mask, returns inverted bit values. |
Provide Feedback