New interrupt dialog for HSC
The
New interrupt
dialog for high-speed counter (HSC) can be accessed by:- InProject Organizer, right-clickPrograms, and then selectNew interrupt.
- InNew interrupt, from theTypelist, selectHigh speed counter (HSC).
Use the
New interrupt
dialog to:- Configure the interrupt properties, such as ID and the program type to use it in.
- Configure the interrupt parameters.
Provide Feedback