HSCCmd values
The following table describes the HSC commands for each HSC command value.
HSC command | Command description |
|---|---|
0x01 | HSC RUN:
|
0x02 | HSC Stop: Stop a HSC counting (if HSC is in Run mode and the rung is enabled). |
0x03 | HSC Load/Set: Reload the HSC Application Data (if rung is enabled) for 6 input elements: HPSetting, LPSetting, HPOutput, LPOutput, OFSetting, and UFSetting. Note: This command does not re-load the input element HSC accumulator. |
0x04 | HSC Accumulator Reset (if rung is enabled). |
Command value | Result | Conditions |
|---|---|---|
HscCmd =1 | Starts the HSC mechanism, and the HSC transitions to running mode. | Setting the Enable input parameter to FALSE does not stop counting while in running mode. HscCmd =2 must be issued to stop counting. |
The HSC mechanism automatically updates values. | HSC AppData.Accumalator is updated with HSC Sts.Accumulator. | |
HscCmd =4 (reset) | Sets the HSC Acc value to the HSC AppData.Accumalator value. | HscCmd =4 does not stop HSC counting. If HSC is counting when HscCmd =4 is issued, some counting might be lost. To set a specific value to HSC Acc while counting, write the value to HSC AppData.Accumalator immediately before HscCmd =4 is issued. |
Provide Feedback