File/Array instructions
Use File/Array instructions to alter the output data to change the status without altering the program.
Instruction | Description |
|---|---|
Calculates a running average over a number of defined samples. |
Provide Feedback