Timer/Counter instructions
Use Timer/Counter instructions to control operations based on the number of events and time.
Instruction | Description |
|---|---|
Counts integers from a given value down to 0, one by one. | |
Counts integers from 0 up to a given value, one by one. | |
Counts integers from 0 up to a given value, one by one, or from a given value down to 0, one by one. | |
Reads the high-speed clock value in the Micro800 controller. | |
Retentive timing. Increases an internal timer when input is active but does not reset the internal timer when input changes to inactive. | |
Off-delay timing. Increase an internal timer up to a given value. | |
On-delay timing. Increase an internal timer up to a given value. | |
Delay turning on an output on a true rung and then delay turning off the output on the false rung. | |
Pulse timing. On a rising edge, increases an internal timer up to a given value. |
Provide Feedback