COM_IO_WDOG
The COM_IO_WDOG instruction monitors external messaging to controller inputs and outputs.
For example, if the CIP write command to variable _IO_EM_DO_00 is not received over EtherNet/IP within the configured timeout, the watch dog timer will expire and all controller outputs are reset.
EtherNet/IP, Modbus TCP, and Modbus RTU protocols are supported.
Languages supported: Function block diagram, ladder diagram, structured text.
This instruction applies to the L20E, L50E, and L70E controllers. The instruction is supported when the firmware revision is 12.00 or later.
COM_IO_WDOG

TIP:
- Although multiple instances of the instruction can exist, only one instance can be enabled. Otherwise, an error with ErrorID set to 2 will occur.
- Only controller embedded, plug-in, and expansion digital I/Os are supported.
Parameter | Parameter Type | Data Type | Description |
|---|---|---|---|
Enable | Input | BOOL |
|
OutputClr | Input | BOOL |
|
PT | Input | TIME | Duration to wait before timeout. The value for a timeout cannot be less than one second, or an error occurs. The maximum value for PresetTime can be the maximum value within TIME data type. |
TimeOut | Output | BOOL |
|
ET | Output | TIME | The current elapsed time. The possible values range is from 0 ms through 1193h2m47s294ms. |
Status | Output | USINT | Status of the function block.
|
Error | Output | BOOL | Indicates an error. |
ErrorID | Output | USINT | When an error occurs, ErrorID contains the error code. |
ErrorID Code | Error Description |
|---|---|
1 | The PresetTime is less than one second. |
2 | Another COM_IO_WDOG function block instance is already executing. |
COM_IO_WDOG examples
COM_IO_WDOG function block diagram example

COM_IO_WDOG ladder diagram example

COM_IO_WDOG structured text example

Provide Feedback