OSR (one shot rising)
The OSR instruction detects a rising edge of a Boolean variable. The OSR block sets output Q for one cycle when input CLK toggles from cleared to set (a rising edge is detected at input CLK).
Languages supported: Function block diagram, ladder diagram, structured text.
This instruction applies to the Micro810, L20E, L50E, and L70E controllers.
OSR

Parameter | Parameter Type | Data Type | Description |
|---|---|---|---|
CLK | Input | BOOL | Any Boolean variable.
|
Q | Output | BOOL |
|
OSR examples
OSR function block diagram example

OSR ladder diagram example

OSR structured text example

Results

(* ST Equivalence: OSR1 is an instance of an OSR block *) OSR1(cmd); nb_edge := ANY_TO_DINT(OSR1.Q) + nb_edge;
Provide Feedback