AHLI data type
Use the following table to determine the parameter values for the AHLI data type.
Parameter | Data Type | Description |
---|---|---|
Channel | UINT | Serial port number:
|
ClrRts | BOOL | Used to reset the RTS control line. |
SetRts | BOOL | Used to set the RTS control line. |
Cancel | BOOL | When this input is set to TRUE, this function block does not execute. |
Provide Feedback