ADD
The ADD instruction adds two or more Integer, Real, Time, or String values.
Languages supported: Function block diagram, ladder diagram, structured text.
This instruction applies to the Micro810, L20E, L50E, and L70E controllers.
ADD

Parameter | Parameter Type | Data Type | Description | |
|---|---|---|---|---|
EN | Input | BOOL | When set to true, the instruction is enabled.
| |
i1 | Input | SINT USINT BYTE INT UINT WORD DINT UDINT DWORD | LINT ULINT LWORD REAL LREAL TIME STRING | Addend of the Real, Time, or String data type. All inputs must use the same data type. |
i2 | Input | SINT USINT BYTE INT UINT WORD DINT UDINT DWORD | LINT ULINT LWORD REAL LREAL TIME STRING | Addend of the Real, Time, or String data type. All inputs must be of the same data type. |
o1 | Output | SINT USINT BYTE INT UINT WORD DINT UDINT DWORD | LINT ULINT LWORD REAL LREAL TIME STRING | Sum of the input values in Real, Time, or String format. Input and output must use the same data type. |
ENO | Output | BOOL | Enables output. Applies to ladder diagram programs. | |
ADD examples
ADD function block diagram example

ADD ladder diagram program example

(* ST equivalence: *) ao10 := ai101 + ai102; ao5 := (ai51 + ai52) + ai53;
Provide Feedback