USB port configuration page
Use the USB Port configuration page to do the following actions:
- Turn on or turn off the USB port.
- View the basic USB port settings.
Setting | Description |
|---|---|
Status | Turns on or turns off the USB port. The USB port is turned on by default. |
Suspend state | Shows the suspended state of the USB port. The USB port is not suspended by default. |
Bus speed | Shows the highest supported USB bus speed. Options are:
Full speed is the default setting. |
Mode | Shows the current mode of the USB port. Options are:
Slave mode is the default setting. |
State | Shows the state of the USB port. Options are:
Ready is the default setting. |
Provide Feedback