Startup/Faults configuration page
Use the
Startup/Faults
configuration page to do the following actions:- Configure the startup settings for theMicro800controller in theFactoryTalk Design Workbenchproject.
- Open the Memory configuration page.
- Open the controller diagnostics view to review memory information for the current project and the project stored in memory.
- Specify the controller behavior when a hard fault occurs.
TIP:
Before changing the
Mode Behavior
and Fault Override
settings, disconnect the controller.Setting | Description |
|---|---|
Diagnose | Opens the Controller Diagnostics view. Diagnose is available when the controller is online. |
Mode Behavior | Specifies the startup behavior of the Micro800 controller on power-up. Options are:
Retain last mode before power-down is the default setting. |
Fault Override | Specifies the fault behavior during controller power-up. Options are:
Do not clear faults is the default setting. |
Hard Fault | Specifies the controller behavior when a hard fault occurs. Options are:
Stop the controller is the default setting. |
Memory Module (L50E and L70E controllers)/Memory Card (L20E controllers) | Displays the message and a link to the memory card or memory module configuration page. The link is available for:
|
Provide Feedback