Serial Port - Modbus RTU configuration page
Use the Modbus RTU configuration page to do the following actions:
- Configure Modbus RTU settings.
- Open the communication diagnostics view by selecting theDiagnosebutton.
The displayed configuration settings vary with the
Micro800
controller selection.Setting | Description |
|---|---|
Common Settings | |
Diagnose | Opens the communication diagnostics view. Diagnose is available when the controller is online and CIP Serial or Modbus RTU is selected as the driver. |
Baud rate | Lists the baud rate in bits per second. Options are:
The default baud rate is 19200. |
Parity | Lists the parity bit usage in the communication packets. Options are:
|
Modbus role | Specifies the role of the Modbus port. Options are as follows:
The default option is Master . |
Unit address | Specifies the Unit ID if configured as a Modbus server (slave). The option is not available when Modbus role is set as Master .When you select Slave or Auto for Modbus role , the unit address is from 1 through 247. The default value is 1 .For instance, in a scenario where the controller is set up as a Modbus RTU slave that is connected to a PanelView™ Component (PVC), the PVC is the Modbus master and uses the address of 0. |
Protocol Control | |
Media | Specifies the supported media types. Available options for L50E and L70E controllers are:
|
Control line | Specifies the type of handshake that is used for communication.
|
Data bits | Specifies the number of data bits per character. The value is 8 and is read-only. |
Stop bits | Specifies the number of stop bits per character. Options include 1 and 2 . 1 is the default option. |
Response timer | Specifies a Modbus master's minimum waiting time for a response from the Modbus slave before a new transmission can begin. The value is from 0 through 4,294,967,295. The default value is 200. In a scenario where the Micro800 controller serves as a master of the Modbus RTU slave, to send a complete response, the value must be restricted within the required time from the slave. |
Broadcast pause | Specifies the amount of time to delay after the data broadcast. The value is from 0 through 4,294,967,295. The default value is 200. |
Inter-frame (delay/timeout) | Specifies the amount of time to delay after a transmission request. The value is from 0 through 4,294,967,295. The default value is 0. |
RTS pre-delay | Specifies the amount of time to delay before requesting a transmission. The option is available when Media is set to RTS32 and Control line is set to RTS/CTS .The value is from 0 through 4,294,967,295. The default value is 0. The option is available when Media is set to RS232 and Control line is set to RTS/CTS . |
RTS post-delay | Specifies the amount of time to delay after requesting a transmission. The option is available when Media is set to RTS32 and Control line is set to RTS/CTS .The value is from 0 through 4,294,967,295. The default value is 0. The option is available when Media is set to RS232 and Control line is set to RTS/CTS . |
Provide Feedback