Serial Port - ASCII configuration page
Use the ASCII configuration page to do the following actions:
- Configure the common ASCII channel settings.
- Configure the ASCII channel protocol control settings.
The displayed configuration settings vary with the
Micro800
controller selection.Setting | Description |
|---|---|
Common Settings | |
Baud rate | Lists the baud rate in bits per second. Options are:
The default value is 19200. |
Parity | Lists the parity bit usage in the communication packets. Options are:
|
Protocol Control | |
Media | Specifies the supported media types. Options are as follows:
When Media is set to RS485 , Control line is defaulted to No handshake . |
Control line | Lists the control line communication options. The options are available when Media is set to RS232 .When Media is set to RS485 , Control line is defaulted to No handshake .
The available options for L20E, L50E, and L70E controllers are as follows:
|
Deletion mode | Lists the options for the ASCII delete character. The mode affects the characters that are echoed back to the remote device.
|
Data bits | Specifies the number of bits of data per character. Options include 7 and 8 . 8 is the default option. |
Stop bits | Specifies the number of stop bits per character. Options include 1 and 2 . 1 is the default option. |
Append chars | Specifies the append characters that are defined for the ASCII protocol and used for transmitting. The range is from zero through two-hexadecimal values, separated by a comma. 0xFF is reserved and can be used to signify no characters. For example:
|
Termination chars | Specifies the termination characters that are defined for the ASCII protocol and used for receiving. The range is from zero through two-hexadecimal values, separated by a comma. 0xFF is reserved and can be used to signify no characters. The default value is 0x0D,0x0A . |
XON/XOFF | Turns on or turns off the XON/XOFF function. It is turned off by default. |
Echo mode | Turns on or turns off character echo. When turned on, all received characters are echoed back to the computer running FactoryTalk Design Workbench . When the Micro800 controller is connected with a terminal, you can view the entered characters.It is turned off by default. |
RTS pre-delay | Specifies the delay period before requesting a transmission. The value is from 0 through 32767, with each unit increment representing 20 milliseconds. The default value is 0. |
RTS post-delay | Specifies the delay period after requesting a transmission. The value is from 0 through 32767, with each unit increment representing 20 milliseconds. The default value is 0. |
Provide Feedback