Remote LCD configuration page
The
remote LCD
configuration page is available for L20E, L50E, and L70E controllers. Use the page to do the following actions:- Open theLCD variablesview to select which variables to monitor using the LCD module.
- Open theSerial Portconfiguration page to view and configure serial port settings.
- Turn on push button key read.
- Specify backlight settings for the LCD.
- Specify a message and the message display settings for the LCD.
Setting | Description |
|---|---|
Configure the serial port for remote LCD | Switches between using the serial port settings and the default Common Industrial Protocol settings for the remote LCD.
Remote LCD settings are used by default. |
Status | Indicates the status of the remote LCD as Connected or Disconnected .
|
LCD variables | Opens the LCD variables view that is available when the controller is offline.Up to 400 variables are supported for the remote LCD display. Exceeding the limit will lead to building problems. |
Hardware Settings | |
Enable push button key read | Turns on or turns off the push button key read for the remote LCD. It is turned on by default. |
Backlight mode | Specifies the backlight behavior for the remote LCD. Options are as follows:
Interval is the default selection. |
Time | Specifies the backlight interval when Backlight mode is set to Interval . The value is from 10 through 120 seconds. The default value is 30. |
Contrast | Specifies the backlight contrast on the LCD. The value is from 0 through 100 percent. The default value is 50 percent. |
Startup Message | |
Display time | Specifies the duration for which the startup message is displayed on the LCD. The value is from 1 through 30 seconds. The default value is 3 seconds. |
Font size | Specifies the font size of the startup message on the LCD. Options are as follows:
Large (8x16 pixels) is the default selection. |
Max size | Shows the maximum length of the startup message based on the Font size selection.The value is read-only. |
Message | Specifies the startup message for the remote LCD. The default startup message is 2080-REMLCD .English characters offer the optimal preview result. |
Preview | Displays the startup message as it appears on the LCD. |
Provide Feedback