Recipe configuration page
The
Recipe
configuration page is available for the following controllers:- L20E
- L50E
- L70E
Up to 10 recipes are supported, with each recipe having up to 50 versions and 128 variables. Having more than 128 variables in a recipe will result in building problems.
Use the
Recipe
configuration page to do the following actions:- Add recipes to or delete recipes from the recipe list.
- Import recipes from or export recipes to an M8A file.
- Open the variable selector to add variables to a recipe.
- Move a recipe's variables up and down in the variable list.
- Delete recipes from a controller.
Setting | Description |
|---|---|
Recipe list | Lists the recipes in the project. Select or clear the RCP<x> checkbox to add the recipe to or remove the recipe from the recipe list. |
Import | Opens Import data log to Import recipes from an M8A file on the computer.Import is available when the controller is offline. |
Export | Export recipes to an M8A file on the controller. Export is available when the following conditions are met:
|
Manage recipes | Performs the following actions on the recipes:
|
Recipe details | Specifies the following information of the recipe:
The dialog is available by clicking beside a selected recipe. |
Provide Feedback
beside a selected recipe.