Download recipes
Use the
<controller-name>: Manage recipes
page to download recipes to the memory card to update the recipes for the controller project.Prerequisites
- The controller is online.
To download recipes
- InProject Organizer, double-click the controller to open the controller application workspace.
- In theControllertree, selectRecipe.
- On theRecipeconfiguration page, selectManage recipes.
- In<controller-name>: Manage recipes, select
. - InDownload recipes to memory card, selectBrowse.
- InSelect folder, find and select the recipe file, and then selectOK.
- InDownload recipes to memory card, selectDownload.
Provide Feedback