Delete recipe files from the controller
Delete the recipe files from the memory card when the recipes are no longer part of the current controller project.
Prerequisites
- The project is online.
- One or more recipes are added.
To delete a recipe set from the controller
- InProject Organizer, double-click the controller to open the controller application workspace.
- In theControllertree, selectRecipe.
- On theRecipeconfiguration page, selectManage recipes.
- In<controller-name>: Manage recipes, select
. - InDelete recipes from memory card, select the recipe files you want to delete, and then selectDelete.
Provide Feedback