Add recipe details
Recipe details are optional configurations for a recipe. Use
Recipe detail
to do the following actions:- Change the character that distinguishes the different recipe fields. Comma is the default separator.
- Add descriptions to a recipe. Up to 100 characters are supported.
Prerequisites
- The project is offline.
To add recipe details
- InProject Organizer, double-click the controller to open the controller application workspace.
- In theControllertree, selectRecipe.
- On theRecipeconfiguration page, from theRecipelist, select the added recipe, and then select
. - InRecipe details, select a separator and enter the description as needed.
- SelectOK.
Provide Feedback