Add variables to a data set
Data logs contain data sets and record the data values of a defined set of variables that you added to the controller project. Use the
Data Log
configuration page to add variables to a data set.Prerequisites
- The controller is offline.
To add variables to a data set
- InProject Organizer, double-click the controller to open the controller application workspace.
- In theControllertree, selectData log.
- On theData Logconfiguration page, select an added data set to which you want to add the variables.
- Double-clickSelect variableor select
to open the variable selector. - In the variable selector, select the variable, and then selectSelect.TIP: To change the order of data set variables, drag the row headers of the variables to the desired place.
Provide Feedback