Add data set details
Data set details are optional configurations for a data set. Use the
Data set details
dialog to do the following actions:- Change the character that separates cells in a data set file. The default separator is comma.
- Add descriptions to a data set. You can enter up to 100 characters.
Prerequisites
- The project is offline.
To add data set details
- InProject Organizer, double-click the controller to open the controller application workspace.
- In theControllertree, selectData Log.
- On theData Logconfiguration page, from theData Loglist, select
beside the data set. - InData set details, select the separator and enter the data set description.
- SelectOK.
Provide Feedback